Load Waveform File
While not connected to an instrument, you can load a previously-saved waveform file from an instrument and view it in the Offline Waveform File Viewer (see below).
Click
, then select "Open Waveform File".
The waveform file is exported from an instrument with a *.h5 file extension and stored on your computer.
When you load a previously-saved waveform file, the file will be opened and stored with a *.ivif file extension on your computer. By default, the file is stored in the "Documents" folder on your computer and are organized by instrument type. For example – C:\Users\<user_name>\Documents\Keysight\PathWaveOscilloscope\Data Logs\.
The original waveform file in *.h5 file extension will remain unchanged.
The original waveform file in *.h5 file extension will remain unchanged.
Offline Waveform File Viewer
| 1 | Configure the traces display settings. See Trace Data Settings Panel. | |
| 2 | View the waveform data information. | |
| 3 | Use Trace Display Toolbar to zoom in/out, and auto scale the displayed data. | |
| 4 | Export a data log from the application to Microsoft Excel (.xlsx) format or CSV (comma-separated values) format. See Export Data Log. |
|
| 5 | Select the chart type. See Data Display Views. | |
| 6 | Show portion of data currently displayed on chart above. See Data Preview Bar. |